Advantech Customize i.mx 6 platfrom with problem of flashing eMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Advantech Customize i.mx 6 platfrom with problem of flashing eMMC

765 次查看
ryanhuang821
Contributor I

We try to flash the (Windows 10 Iot Core) ffu file into the eMMC under winPE following the user manual.

We get a error: 31(A device attached to the system is not functioning.) when we execute the command.

Dism.exe /Apply-Image /ImageFile:"C:\Flash.ffu" /ApplyDrive:\\.\PhysicalDrive1 /SkipPlatformCheck

//====================error=========================

2018-09-14 22:35:09, Error DISM DISM FFU Provider: Anti-theft check failed because the machine uses legacy BIOS.
2018-09-14 22:35:09, Error DISM DISM FFU Provider: PerformValidation#505 failed with 0x8007001f.
2018-09-14 22:35:09, Error DISM DISM FFU Provider: FfuApplyInternal#600 failed with 0x8007001f.
2018-09-14 22:35:09, Error DISM DISM FFU Provider: FfuApplyImage#53 failed with 0x8007001f.
2018-09-14 22:35:09, Error DISM DISM FFU Provider: PID=1860 TID=1864 onecore\base\ntsetup\opktools\dism\providers\ffuprovider\dll\ffumanager.cpp:514 - CFfuManager::Apply(hr:0x8007001f)
2018-09-14 22:35:09, Error DISM DISM FFU Provider: PID=1860 TID=1864 onecore\base\ntsetup\opktools\dism\providers\ffuprovider\dll\ffumanager.cpp:424 - CFfuManager::ApplyImage(hr:0x8007001f)
2018-09-14 22:35:09, Error DISM DISM Imaging Provider: PID=1860 TID=1864 onecore\base\ntsetup\opktools\dism\providers\imagingprovider\dll\genericimagingmanager.cpp:2853 - CGenericImagingManager::InternalCmdFFUApply(hr:0x8007001f)
2018-09-14 22:35:09, Error DISM DISM Imaging Provider: PID=1860 TID=1864 onecore\base\ntsetup\opktools\dism\providers\imagingprovider\dll\genericimagingmanager.cpp:547 - CGenericImagingManager::ExecuteCmdLine(hr:0x8007001f)
2018-09-14 22:35:09, Info DISM DISM.EXE: Image session has been closed. Reboot required=no.

 

We attach the dism log.

Thank you.

 
0 项奖励
回复
0 回复数