About the state of pins for LCDIF of i.MX283 during reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the state of pins for LCDIF of i.MX283 during reset

Jump to solution
569 Views
yuuki
Senior Contributor II

Dear Freescale TIC,

I would like to maintain pins of LCDIF in the Low state until the power supply of a LCD module is stabilized.


Are the following pins in a Low state after Reset and during Reset?

・LCD_DATA[17..0」
・LCD_VSYNC
・LCD_HSYNC
・LCD_CLK
・LCD_ENABLE

Best Regards,

Labels (1)
0 Kudos
1 Solution
484 Views
Yuri
NXP Employee
NXP Employee

From section 8.1 (Pin Descriptions Overview) of the i.MX28 Reference Manual :

"Almost all digital pins are powered down (that is, high impedance)

or configured as GPIO input at reset, until reprogrammed. The only

exceptions are TEST PINS(TESTMODE, DEBUG, JTAG pins). These pins

are always active."

View solution in original post

0 Kudos
1 Reply
485 Views
Yuri
NXP Employee
NXP Employee

From section 8.1 (Pin Descriptions Overview) of the i.MX28 Reference Manual :

"Almost all digital pins are powered down (that is, high impedance)

or configured as GPIO input at reset, until reprogrammed. The only

exceptions are TEST PINS(TESTMODE, DEBUG, JTAG pins). These pins

are always active."

0 Kudos