About the meta-fsl-bsp-release layer in freescale-imx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the meta-fsl-bsp-release layer in freescale-imx

跳至解决方案
4,053 次查看
jasonl
Contributor II

Hello there,

I am trying to include imx layer into our yocto build but unfortunately, the environment is a bit different. The gstreamer1.0_1.8.1.bb file (or more)   in meta-fsl-bsp-release  is hard-coded as FILESEXTRAPATHS_prepend := "${BSPDIR}/sources/poky/meta/recipes-multimedia/gstreamer/files:". But most of the project I have seen they most likely use the path like "~/${DIR}/poky/meta".

Is it possible to change that upstream?

Thanks,

Jason

标记 (2)
1 解答
1,830 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jason Liu,

The meta-fsl-bsp-release layer is part of the BSP Release, so this layer is not part of the Community BSP wich is part of the Yocto Project (Open Source), that’s why this path is different from other layers.

You can see how the layers are stacked on the following document, it’s not very recent but the basis structure remains.

https://community.nxp.com/docs/DOC-102993

I hope this helps!

Regards,

在原帖中查看解决方案

1 回复
1,831 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jason Liu,

The meta-fsl-bsp-release layer is part of the BSP Release, so this layer is not part of the Community BSP wich is part of the Yocto Project (Open Source), that’s why this path is different from other layers.

You can see how the layers are stacked on the following document, it’s not very recent but the basis structure remains.

https://community.nxp.com/docs/DOC-102993

I hope this helps!

Regards,