About input voltage of VDD_SNVS_IN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About input voltage of VDD_SNVS_IN

752 Views
okamotosatoshi
Contributor IV

I want to check for VDD_SNVS_IN using a coin battery.

During normal operation, VDD_SNVS_IN is the operating range is 2.9V ~ 3.3V.

- i.MX 6Solo/6DualLite Applications Processors for Consumer Products, Rev. 5 4.1.3 Operating Ranges

As an example, it shows the discharge characteristic graph of the ML621.

Immediately, coin battery is reduced to about 2.5V.

In addition, less than the operating range and supplies using the PMIC (MMPFxxxx).

ML621_Discharge.png

If you want to back up the RTC in the Coin Cell Mode, operating  range of VDD_SNVS_IN will be 2.9V ~ 3.3V?

Regards,

-satoshi

Labels (2)
0 Kudos
4 Replies

570 Views
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for answering.

I consider the configuration of the backup circuit.

It became the future of help.

Regards,

-satoshi

0 Kudos

570 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Strictly speaking, You are right, VDD_SNVS_IN operating range from 2.9 V  provides

difficulties for battery selection and using, when we should take into account battery

discharging. Nevertheless, the value of 2.9 V is correct. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

570 Views
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for answering.

It may be difficult itself to back up the RTC(in IMX) in the coin battery.

I want you to presentation if there is a reference circuit of the RTC backup.

(Reference circuit you do not want to use the PMIC.)

Regards,

-satoshi

0 Kudos

570 Views
Yuri
NXP Employee
NXP Employee

Hello, Satoshi !

     SABRE SD Board / Platform design may be used as reference, but

it is based on PMIC. No i.MX6 designs without PMIC from NXP.
Basically it is possible to connect i.MX6 VDD_SNVS_IN with a battery directly.

Regards,
Yuri.

0 Kudos