About WDOG_B signal by the software for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About WDOG_B signal by the software for i.MX6

Jump to solution
908 Views
yuuki
Senior Contributor II

Dear all,

According to session WDOG_B generation of the reference manual, software is able to assert the WDOG_B signal by writing the WDA bit of WDOG_WCR register.

In this case, is the system reset?
Or is only WDOG_B signal asserted ?

May I have advice?

Best Regards,
Yuuki

Labels (1)
Tags (3)
0 Kudos
1 Solution
506 Views
Yuri
NXP Employee
NXP Employee

  Only the WDOG_B signal is asserted.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
507 Views
Yuri
NXP Employee
NXP Employee

  Only the WDOG_B signal is asserted.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos