hello,Community
About SD / MMC manufacture boot flow in Figure 6-46
When SDMMC MFG mode is enabled,
Even if it is Serial Downloader, will it start with SDMMC MFG mode boot?
How can I disable SDMMC MFG mode?
Which pin is it?
How is it processed (PU or PD)?
best regards
Goto
Hello,
Table 6-25. DISABLE_SDMMC_MFG column in Boot eFUSE descriptions has Yes in the GPIO column, and the note has the following description.
This setting can be overridden by the GPIO settings when the BT_FUSE_SEL fuse is intact.See GPIO Boot Overrides for
the corresponding GPIO pin.
It may be possible to disable the SD / MMC MFG mode by pulling up one of BOOT_CFG [0] to [19].
If possible, please tell me the CFG No.
best regards
Goto
please refer to picture below (there is no option for GPIO override):
Best regards
igor
hello,
6.6.2.5 Internal Boot mode
There is a description in Reference 1 below, and “Yes” in the GPIO column of DISABLE_SDMMC_MFG column in Table 6-25. Boot eFUSE descriptions, and Reference 2 below in the note.
What is different from the answer (picture below (there is no option for GPIO override))?
Reference 1
• If BT_FUSE_SEL = 0, the specific boot configuration parameters may be set using the GPIO pins rather than eFUSEs.The fuses that can be overridden when in this mode are indicated in the GPIO column of Table 6-25.Table 6-26 provides the details of the GPIO pins.
Reference 2
This setting can be overridden by the GPIO settings when the BT_FUSE_SEL fuse is intact.See GPIO Boot Overrides for the corresponding GPIO pin.
best regards
Goto
there is no option for GPIO override for disabling SDMMC MFG mode.
Best regards
igor
Hi Goto
for disabling SDMMC MFG mode it is necessary to burn fuse
described in Table 6-17. Boot Fusemap i.MX 7Dual Applications Processor Reference Manual
Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog
>Even if it is Serial Downloader, will it start with SDMMC MFG mode boot?
yes
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------