About MMDC Profiling Tool for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MMDC Profiling Tool for i.MX6

3,564件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We want to check a operating rate of CPU and GPU.
We used mmdc2 command.

We have some questions about MMDC Profiling.

<Q1>
About the result of the following command.
What does Utilization mean?
Is it the average of the operation rate of CPU#0 and CPU#2?

================================================
root@imx6qdlsolo:/unit_tests# ./mmdc2
i.MX6DL detected.
MMDC SUM

MMDC new Profiling results:
***********************
Measure time: 500ms
Total cycles count: 198076320
Busy cycles count: 30948398
Read accesses count: 739442
Write accesses count: 955
Read bytes count: 47310392
Write bytes count: 30560
Avg. Read burst size: 63
Avg. Write burst size: 32
Read: 90.24 MB/s / Write: 0.06 MB/s Total: 90.30 MB/s
Utilization: 9%
Overall Bus Load: 15%
Bytes Access: 63
================================================


Furthermore, we tried the following command.

<Q2>
About the result of the following command.
Does this show a profiling result of CPU#0?

================================================
root@imx6qdlsolo:/unit_tests# ./mmdc2 ARM
i.MX6DL detected.
MMDC ARM

MMDC new Profiling results:
***********************
Measure time: 500ms
Total cycles count: 198083214
Busy cycles count: 30898478
Read accesses count: 3738
Write accesses count: 552
Read bytes count: 228288
Write bytes count: 17664
Avg. Read burst size: 61
Avg. Write burst size: 32
Read: 0.44 MB/s / Write: 0.03 MB/s Total: 0.47 MB/s
Utilization: 0%
Overall Bus Load: 15%
Bytes Access: 57
================================================

<Q3>
If <Q2> is Yes,
Can we check Profiling of CPU#0 and CPU#1 separately?


<Q4>
According to the source code of the mmdc command, it seems to refer to AXI_ID
We referred to a reference manual.

IMX6SDLRM Rev. 2, 04/2015:
- "Table 45-10. i.MX 6Solo/6DualLite AXI ID" (P.3930)

However, AXI_ID for GPU3D1, GPU3D2 and VPU is not explained.
Would you tell me these AXI_ID?

May I have advice?

Best Regards,
Yuuki

ラベル(3)
0 件の賞賛
2 返答(返信)

1,893件の閲覧回数
sergkot
Contributor II

yuuki‌ Have you found how to fix the strange result? May be it is a normal, but I am not sure.

0 件の賞賛

1,893件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

 

  The MMDC Profiling tool uses the Profiling Control Registers. Please refer to
section 45.7 (MMDC Profiling) of i.MX 6Solo/6DualLite Applications Processor
Reference Manual, Rev. 2, 04/2015.

 

  MMDC source code may be found in the tests package.

 

< http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz >

 

Hope the sources help to clarify parameters, provided by the Profiling tool.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛