About CLKx_N voltage range in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About CLKx_N voltage range in i.MX6DQ.

Jump to solution
510 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to Table 2-7. Oscillator and clock recommendations in Hardware Development Guide for i.MX 6, Rev. 1.

There is below description.

======

Alternatively, a single-ended signal can be used to

drive a CLKx_P input. In this case, the corresponding

CLKx_N input should be tied to a constant voltage

level equal to 50% of VDD_HIGH_CAP.

======

How much is the deviation of the CLKx_N voltage permissible?

Do you have voltage range of CLKx_N?

Best Regards,

Keita

Labels (3)
0 Kudos
1 Solution
462 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

TIA/EIA-644 standard.sect.4.2.4

defines allowable common voltage range as

+0.050 V to +2.350 V . So this voltage can be applied

to CLKx_N.

Best regards

igor
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
463 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

TIA/EIA-644 standard.sect.4.2.4

defines allowable common voltage range as

+0.050 V to +2.350 V . So this voltage can be applied

to CLKx_N.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos