Hi,
I am trying to play 4k video on a 4k display using imx8m evk on kernel release 4.14.78ga. on checking the FB mode using fbset command,
mode "3840x2160"
geometry 3840 2160 3840 2160 32
timings 0 0 0 0 0 0 0
accel true
rgba 8/16,8/8,8/0,0/0
endmode
But when I play a video it plays fine on terminal without error, but can't see any frame on display. On booting I can't see a desktop screen too. Is there something I am missing. As according to release note, 4k should be working on primary HDMI. On loading dual display dtb again 4k display won't show any thing on screen. Please help me with this.
已解决! 转到解答。
Hi sandeep
one can try Demo Images from link
and gstreamer pipeline:
gst-launch-1.0 filesrc location=file.mp4 ! video/quicktime ! qtdemux ! queue ! vpudec ! queue ! kmssink force-hantrotile=true
other useful links :
https://community.nxp.com/docs/DOC-343017
Yocto release for i.MX 8MQ - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi sandeep
one can try Demo Images from link
and gstreamer pipeline:
gst-launch-1.0 filesrc location=file.mp4 ! video/quicktime ! qtdemux ! queue ! vpudec ! queue ! kmssink force-hantrotile=true
other useful links :
https://community.nxp.com/docs/DOC-343017
Yocto release for i.MX 8MQ - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I have tried to test 4k video using gstreamer pipeline on demo images for following releases:
* 4.9.51
* 4.6.88
* 4.14.62
* 4.14.78
* 4.14.98
But as result Display shows nothing and on display it a msg appears as "No signal".
Is it possible that my 4k TV(display) is not compatible. If so can you suggest a display with brand and module No. on which you have tested. I will try to arrange that same module TV.
yes one can try other monitors, for example one can look on
Hi,
I was able to check 4k video on other TV, and was able to play video.
On playing video in standard dtb video plays with 10 fps.
On playing with dual display dtb, video still plays better but 20fps only as "force-hantrotile=true" option is available.
Have you seen why by playing a video of 60fps and 30 fps. What was the out-come. in both dual and single display scenario.
How can I improve this. Or this is a limitation.
video link I tried is,
http://distribution.bbb3d.renderfarming.net/video/mp4/bbb_sunflower_2160p_30fps_normal.mp4
http://distribution.bbb3d.renderfarming.net/video/mp4/bbb_sunflower_2160p_60fps_normal.mp4
Hi sandeep
officially supported resolutions are described in Linux document
Release Notes, Video codec specifications section
Linux L4.14.98_2.0.0 Documentation
for dual case supported: 4k@60fps + HD@60fps using:
gst-launch-1.0 filesrc location=file_4k.mp4 typefind=true ! video/quicktime ! qtdemux ! queue max-size-time=0 ! vpudec ! queue max-size-time=0 ! kmssink force-hantrotile=true sync=false &
gst-launch-1.0 filesrc location=file_HD.ts ! video/mpegts ! tsdemux ! queue max-size-time=0 ! vpudec ! queue max-size-time=0 ! waylandsink
Also may be useful:
https://community.nxp.com/docs/DOC-343017
Best regards
igor