Hi,
Can i.mx6 Quad capture 2 video input of 720P@30 each simultaneously ? Can it be done with CSI ? Can it be done with parallel ?
Regards,
Shabbir
Hi Shabbir
yes it can. Performance is given in IMX6DQRM 37.1.2.1.1 Camera Ports:
for parallel interface, the maximum speed of the interface is 240Mhz.
for MIPI for 4 data lanes configuration : 400MByte/sec
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------