1.2GHz products of i.MX6D/Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1.2GHz products of i.MX6D/Q

ソリューションへジャンプ
964件の閲覧回数
torus1000
Contributor V

Hi.

I guess at least 3 modifications required for 1.2GHz i.MX6D/Q.

    a.  add "ldo_active=on" in u-boot cmdline

    b.  LDO input range: 1.4- 1.5V

    c.  LDO output: 1.275V

*Where CPUFREQ driver read the dtb to support setpoints for b. and c. which programmed in the <kernel>/arch/arm/boot/dts/*.dtsi.

(Q1) Is there any application note or design guide which described tips to modify software and hardware for 1.2GHz i.MX6D/Q?

(Q2) Where can I get the official data sheet for 1.2GHz i.MX6D/Q?

I heard datasheet addendum for it long time ago.

(Q3) Which PMIC/voltage setting scenario as following is recommend for 1.2GHz i.MX6D/Q?

    d. MMPF0100F0/F1..FAxxx: SW1 supply 1.375V to the ARM core at early boot then switch SW1 to 1.4V output.

    e. MMPF0100NPxxx: otp programmed as SW1 supply 1.4V and DCD customized to 1.2GHz for ARM clock.

Can anyone help me?

BR

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
858件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I believe these 3 modifications are correct.

1 unfortunately I am not aware of such documents

2 please create service request

3  "d"

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
859件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I believe these 3 modifications are correct.

1 unfortunately I am not aware of such documents

2 please create service request

3  "d"

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信