請問i.MX283: 1.是不是沒有support Ethernet MII interface. 2.SPI NOR Flash 是不是只能接SSP2 port? 3. 如果同時support NAND Flash and SPI NOR Flash, UART是不是只剩下3 port可以用?
ok, thanks.
Hi OA
i.MX283 supports NAND,SPI-NOR,UART,Ethernet connections and
its specific differencies can be found in
IMX28CEC Table 2. i.MX28 Functional Differences
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
refer to IMX28CEC.PDF Page65, 4.5 i.MX283 Ball Map; some of MII function of i.MX283 are NC pin, could you help how to connection for Ethernet MII function?
Hi OA
you are right: ENET0_TXD2,3 ENET0_RXD2,3 are not
available on i.MX283. So seems MII is not possible with i.MX283.
~igor