如何設計其它的uart

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

如何設計其它的uart

跳至解决方案
1,523 次查看
陳冠儒
Contributor IV

Hi,大家:

小弟有些code設計的問題想請教大家一下,因為我在L3.10.53 BSP source code中imx6qdl-sabresd.dtsi()只有看到uart1的設計,如下:

&uart1 {

pinctrl-names = "default";

pinctrl-0 = <&pinctrl_uart1_1>;

status = "okay";

};

那我若是有新硬體uart2、uart4、uart5(各含有TX,RX,RTS,CTS  4個信號),那我應該怎麼設計code比較好呢?因為原始code寫法是針對debug prot(TX,RX)設計,故不知能直接拿來用嗎?

例如:

寫一個很像的

&uart2 {

pinctrl-names = "default";

pinctrl-0 = <&pinctrl_uart2_1>;

status = "okay";

};

這樣不知道可否?

然後在原始code  mx6sabresd.c中如下:

iomux_v3_cfg_t const uart1_pads[] = {

MX6_PAD_CSI0_DAT10__UART1_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

MX6_PAD_CSI0_DAT11__UART1_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

};

我可以多寫一個如下的設定嗎:

iomux_v3_cfg_t const uart2_pads[] = {

MX6_PAD_CSI0_DAT14__UART2_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

MX6_PAD_CSI0_DAT15__UART2_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

MX6_PAD_CSI0_DAT18__UART2_RTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),

MX6_PAD_CSI0_DAT19__UART2_CTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),

};

然後這又該如何驅動呢?因為uart1靠如下驅動:

static void setup_iomux_uart(void)

{

imx_iomux_v3_setup_multiple_pads(uart1_pads, ARRAY_SIZE(uart1_pads));

}

還是不能這樣寫,再麻煩大家幫忙一下了,感謝大家。

(初學修改code,不是很熟,請大家見諒~~~)

标签 (4)
1 解答
1,147 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 陳 冠儒

for other uarts examples one can at sabreai dts files, imx6qdl-sabreauto.dtsi:

Linux/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi - Linux Cross Reference - Free Electrons

Linux/Documentation/devicetree/bindings/serial/fsl-imx-uart.txt - Linux Cross Reference - Free Elect...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,148 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 陳 冠儒

for other uarts examples one can at sabreai dts files, imx6qdl-sabreauto.dtsi:

Linux/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi - Linux Cross Reference - Free Electrons

Linux/Documentation/devicetree/bindings/serial/fsl-imx-uart.txt - Linux Cross Reference - Free Elect...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,147 次查看
陳冠儒
Contributor IV

hi,igorpadykov:

thanks for you help,sorry .

Article, I do not see very clearly.

how to do is write the article.

tnanks for you.

0 项奖励
回复
1,147 次查看
陳冠儒
Contributor IV

0 项奖励
回复