如何在同一台电脑上使用ltib使其既可以编译mpc8313又可以编译ixm6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

如何在同一台电脑上使用ltib使其既可以编译mpc8313又可以编译ixm6

470 Views
yeyue
Contributor II

先前在一台装了ubuntu10.04的电脑上安装了ltib编译mpc8313,

现在我想在同一台电脑上使用ltib编译imx6。

这样做会不会有问题?

如果没有问题该如何配置?

谢谢

0 Kudos
1 Reply

398 Views
igorpadykov
NXP Employee
NXP Employee

Hi ye

in general both ltibs for mpc8313 and i.MX6 can work on one

computer, though recommended not to mix them.  Below

link may be helpful with building issues with i.MX ltibs:

Re: ltib installation problem in i.mx28

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos