i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) and i.MX7ULP1 PRC2(Beta2) Release Announcement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) and i.MX7ULP1 PRC2(Beta2) Release Announcement

i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) and i.MX7ULP1 PRC2(Beta2) Release Announcement

The Linux L4.9.11_1.0.0 RFP(GA) for i.MX6 release files are now available on www.nxp.com 

 

  • Files available:

#

Name

Description

1

L4.9.11_1.0.0-ga_images_MX6QPDLSOLOX.tar.gz

i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files

2

L4.9.11_1.0.0-ga_images_MX6SLEVK.tar.gz

i.MX 6Sololite EVK Linux Binary Demo Files

3

L4.9.11_1.0.0-ga_images_MX6UL7D.tar.gz

i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files

4

L4.9.11_1.0.0-ga_images_MX6SLLEVK.tar.gz

i.MX 6SLL EVK Linux Binary Demo Files

5

L4.9.11_1.0.0-ga_images_MX7ULPEVK.tar.gz

i.MX 7ULP EVK Linux Binary Demo Files 

6

L4.9.11_1.0.0-ga_mfg-tools.tar.gz

i.MX Manufacturing Toolkit for Linux L4.9.11_1.0.0 BSP

7

L4.9.11_1.0.0-ga_gpu-tools.tar.gz

L4.9.11_1.0.0 i.MX VivanteVTK file

8

bcmdhd-1.141.100.6.tar.gz

The Broadcom firmware package for i.MX Linux L4.9.11_1.0.0 BSP.

9

imx-aacpcodec-4.2.1.tar.gz

Linux AAC Plus Codec for L4.9.11_1.0.0

10

fsl-yocto-L4.9.11_1.0.0.tar.gz

L4.9.11_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide.

 

  • Target boards:
    • i.MX 6QuadPlus SABRE-SD Board and Platform
    • i.MX 6QuadPlus SABRE-AI Board
    • i.MX 6Quad SABRE-SD Board and Platform
    • i.MX 6DualLite SABRE-SD Board
    • i.MX 6Quad SABRE-AI Board
    • i.MX 6DualLite SABRE-AI Board
    • i.MX 6SoloLite EVK Board
    • i.MX 6SoloX SABRE-SD Board
    • i.MX 6SoloX SABRE-AI Board
    • i.MX 7Dual SABRE-SD Board
    • i.MX 6UltraLite EVK Board
    • i.MX 6ULL EVK Board
    • i.MX 6SLL EVK Board
    • i.MX 7ULP EVK Board (Beta Quality)

 

  • What’s New/Features:

Please consult the Release Notes.

 

  • Known issues

For known issues and more details please consult the Release Notes.

 

  • More information on changes, see:

README: https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/tree/README?h=imx-morty

ChangeLog: https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/tree/ChangeLog?h=imx-morty

标记 (1)
评论

the mfgtool use in WIN10,  when detect the device ,the mfgtool stop

Qt为什么不是5.9呢,能不能升级到5.9 Qtwayland相对完善

FYI:

If you download L4.9.11_1.0.0-ga_images_MX6UL7D.tar from the official IMX7D Sabre board, and try to flash the SD card image, this does not boot. (The uboot is wrong)

The old image L4.1.15_1.2.0-ga_images_MX7DSABRESD.tar.tz does at least have working uboot.

You could of course build an flash the correct uboot.imx onto the SD card (which then works, since the rest of the data is ok), but this is not particularly user-friendly for an EVK image.

无评分
版本历史
最后更新:
‎09-29-2017 12:01 AM
更新人: