The Linux L4.9.11_1.0.0 RFP(GA) for i.MX6 release files are now available on www.nxp.com
# | Name | Description |
1 | i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files | |
2 | i.MX 6Sololite EVK Linux Binary Demo Files | |
3 | i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files | |
4 | i.MX 6SLL EVK Linux Binary Demo Files | |
5 | i.MX 7ULP EVK Linux Binary Demo Files | |
6 | i.MX Manufacturing Toolkit for Linux L4.9.11_1.0.0 BSP | |
7 | L4.9.11_1.0.0 i.MX VivanteVTK file | |
8 | The Broadcom firmware package for i.MX Linux L4.9.11_1.0.0 BSP. | |
9 | Linux AAC Plus Codec for L4.9.11_1.0.0 | |
10 | L4.9.11_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. |
Please consult the Release Notes.
For known issues and more details please consult the Release Notes.
README: https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/tree/README?h=imx-morty
ChangeLog: https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/tree/ChangeLog?h=imx-morty
the mfgtool use in WIN10, when detect the device ,the mfgtool stop
Qt为什么不是5.9呢,能不能升级到5.9 Qtwayland相对完善
FYI:
If you download L4.9.11_1.0.0-ga_images_MX6UL7D.tar from the official IMX7D Sabre board, and try to flash the SD card image, this does not boot. (The uboot is wrong)
The old image L4.1.15_1.2.0-ga_images_MX7DSABRESD.tar.tz does at least have working uboot.
You could of course build an flash the correct uboot.imx onto the SD card (which then works, since the rest of the data is ok), but this is not particularly user-friendly for an EVK image.