Q&A: Is it possible to connect a MIPI CSI-1 device to our i.MX6 MIPI CSI-2 interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Q&A: Is it possible to connect a MIPI CSI-1 device to our i.MX6 MIPI CSI-2 interface?

Q&A: Is it possible to connect a MIPI CSI-1 device to our i.MX6 MIPI CSI-2 interface?

Question:

Is SN65LVDS315 (MIPI CSI-1) compatible with our i.MX6 MIPI CSI-2 interface? CSI-2 extends CSI-1 with multiple lanes, but both standards use the same D-PHY layer.

Answer:

No, the i.MX6 MIPI CSI-2 interface is not compatible with CSI-1 devices.

Standards that require backward compatibility to legacy standards always state that the standards are backward compatible. The CSI-2 standard does not say that. (I have a copy of the standard and I have read it specfically for that reason)  The CSI-2 standard does say that a specifically designed PHY, built to D-PHY MIPI01 specification is used for CSI-2. The PHY's used for CSI-1 and CSI-2 are different and they are not compatible. There are some processors that do have compatiblity for CSI-1 and CSI-2, but if you read closer, you will find that they have two different modes (and probably two different sets of pins): One for CSI-2 and One for CSI-2/CSI-1 legacy. It is interesting that a company would choose to inlcude a dying technology in a newer processor, but my guess is that they have a number of other CSI-1 devices they are trying to sell before they can't be used anywhere and nobody wants them.

if the customer is looking for a parallel camera interface to CSI-2 converter IC, may I recommend the Toshiba TC358746 device. I have not used it specifically, but I have worked with a Toshiba rep on an HDMI to MIPI CSI-2 project that input into the i.MX6 processor. Once all the correct parameters were determined, it worked very well. Much higher data rate flow.

标签 (1)
标记 (1)
无评分
版本历史
最后更新:
‎09-23-2013 01:41 AM
更新人: