BSP: L6.1.22_2.0.0
Platform: i.MX93
Links:
https://github.com/NXP/swupdate-scripts
https://github.com/nxp-imx-support/meta-swupdate-imx
The AN13872 provides us the swupdate yocto layer, swupdate-scripts and test steps, but there is still much to add. The purpose of this knowledge base is to provide customized advice.
As meta-swupdate-imx only provide kirkstone version, we can upgrade or degrade it based on this version. We will take L6.1.22_2.0.0 porting steps as an example.
cd imx-yocto-bsp/sources
git clone https://github.com/sbabic/meta-swupdate.git -b mickledore
git clone https://github.com/nxp-imx-support/meta-swupdate-imx.git
imx-yocto-bsp/sources/meta-swupdate-imx/conf/layer.conf
You can find swupdate version in imx-yocto-bsp/sources/meta-swupdate/recipes-support/swupdate/
About patchs in sources/meta-swupdate-imx/recipes-bsp/u-boot/files/ and imx-yocto-bsp/sources/meta-swupdate-imx/recipes-support/swupdate/files/, you need use devtool to unpack uboot and swupdate into workspace and add changes manunally for development.
CONFIG_ENV_OFFSET_REDUND=CONFIG_ENV_OFFSET+CONFIG_ENV_SIZE
sources/meta-swupdate-imx/recipes-bsp/u-boot/u-boot-imx_%.bbappend
Use uuu or dd command, just like common imx-image-xxx
You can modify partition table refer the size of images. For different soc, the first offset is different. If you are porting i.MX8MP based on iMX8MM, the offset should be 32K.
3.2.1 This error indicates that you need enlarge size of rootfs.
e2fsck 1.45.5 (07-Jan-2020)
The filesystem size (according to the superblock) is 887599 blocks
The physical size of the device is 768000 blocks
Either the superblock or the partition table is likely to be corrupt!
Abort<y>?
3.2.2 You need upgrade e2fsck verison.
e2fsck 1.46.5 (30-Dec-2021)
/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4 has unsupported feature(s): FEATURE_C12
e2fsck: Get a newer version of e2fsck!
/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4: ********** WARNING: Filesystem still has errors **********
resize2fs 1.46.5 (30-Dec-2021)
resize2fs: Filesystem has unsupported feature(s) (/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_ass
solution:
wget https://mirrors.edge.kernel.org/pub/linux/kernel/people/tytso/e2fsprogs/v1.47.0/e2fsprogs-1.47.0.tar.xz
tar -xf e2fsprogs-1.47.0.tar.xz
cd e2fsprogs-1.47.0/
./configure
make -j16
sudo make install
3.2.3 mtools
/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 58: mdir: command not found
/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found
/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found
/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 68: mdir: command not found
solution: sudo apt-get install mtools
Hello,
I am trying to integrate meta-swupdate to Yocto Linux BSP Linux 6.1.22_2.0.0 for a custom board based on i.MX6ULL processor. I followed this document for porting. I am using the meta-swupdate layer from here.
When I build and run the generated image on the custom board, I have observed that the kernel booting hangs after swupdate.service starts. I have raised a ticket in NXP community for the same, https://community.nxp.com/t5/i-MX-Processors/Kernel-booting-hangs-after-swupdate-service/td-p/172042.... I have attached the booting logs and the defconfig file used for swupdate in the ticket. I am not able to attach them here, so referenced the link here.
Any help would be appreciated
Thanks in advance.
Regards
Meetali Patel