FAQ All Boards GPIO Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FAQ All Boards GPIO Test

No ratings

FAQ All Boards GPIO Test

Although you can develop your own driver to control GPIOs inside kernel space, there is a much simpler way for accessing GPIOs from user space. When timing requirements are not an issue, you are able to use GPIO-SYSFS.

SYSFS is a virtual file system that exports some kernel internal framework functionalities to user space and GPIO is one of the frameworks that can have functionalities exported through SYSFS.

The GPIO-SYSFS feature is available in all mainline kernels from 2.6.27 onwards.

Configuring Kernel to export GPIO through SYSFS

To enable GPIO in SYSFS, select the following kernel option:

Device Drivers --->       --- GPIO Support             [*] /sys/class/gpio/... (sysfs interface)

If you are using i.MX233 or i.MX28, after recompiling the kernel, do not forget to generate boot streams again, because this is not automatic even in ltib.

Be sure that the pins you will try to use are really accessible as GPIO pins and were not requested by the kernel (gpio_request). If pin was gpio_request'ed, you will need to gpio_export the same pin inside the kernel in order to have it accessible through SYSFS. If pin is not set as GPIO by default, you will need to set IO MUX in the proper file inside <kernel>/arch/arm/mach-XXX.

Accessing GPIO in user space

After enabling GPIO-SYSFS feature, you can boot your device with the new kernel to make some tests.

First you need to export the GPIO you want to test to the user space:

echo XX > /sys/class/gpio/export

XX shall be determined by the following algorithm:

GPIOA_[B] is the GPIO you want to export, where "A" is the GPIO bank and "B" is the offset of the pin in the bank. if the first available GPIO bank is 0 // (iMX.28, for example)     XX = A*32 + B; else // first GPIO bank is 1     XX = (A-1)*32 + B;

After exporting a GPIO pin, you shall be able to see the GPIO interface exported to:

/sys/class/gpio/gpioXX

Through this interface, you are now able to do things like:

# Reading the pin value cat /sys/class/gpio/gpioXX/value # Changing pin direction echo in > /sys/class/gpio/gpioXX/direction echo out > /sys/class/gpio/gpioXX/direction # Toggling GPIO output level echo 0 > /sys/class/gpio/gpioXX/value echo 1 > /sys/class/gpio/gpioXX/value

It is important to note that through the GPIO virtual filesystem it is only possible to deal with one GPIO pin at a time (per command).
Tags (1)
Comments

This could be a stupid question, but how can I know which pin is physically linked to gpioXX ?

Version history
Last update:
‎09-10-2020 01:41 AM
Updated by: