All Board Android Getevent

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

All Board Android Getevent

All Board Android Getevent

The getevent function shows kernel events like press button events, touchscreen events, sensor events (like accelerometers or magnetometers).

bash-3.2# getevent -h

Usage: getevent [-t] [-n] [-s switchmask] [-S] [-v [mask]] [-p] [-q] [-c count] [-r] [device]

      -t: show time stamps

      -n: don't print newlines

      -s: print switch states for given bits

      -S: print all switch states

      -v: verbosity mask (errs=1, dev=2, name=4, info=8, vers=16, pos. events=32)

      -p: show possible events (errs, dev, name, pos. events)

      -q: quiet (clear verbosity mask)

      -c: print given number of events then exit

      -r: print rate events are received

Bellow an example of all events on some board

bash-3.2# getevent -p

add device 1: /dev/input/event2

  name:    "mxc_ts"

  events:

      SYN (0000): 0000  0001  0003

      KEY (0001): 014a

      ABS (0003): 0000  value 0, min 0, max 0, fuzz 0 flat 0

                        0001  value 0, min 0, max 0, fuzz 0 flat 0

                        0018  value 0, min 0, max 0, fuzz 0 flat 0

could not get driver version for /dev/input/mouse0, Not a typewriter

add device 2: /dev/input/event1

  name:    "mxc_power_key"

  events:

    SYN (0000): 0000  0001

    KEY (0001): 003e

add device 3: /dev/input/event0

  name:    "mxckpd"

  events:

    SYN (0000): 0000  0001

    KEY (0001): 0002  0003  0004  0005  003b  003c  003d  003e

                      0066  0067  0069  006a  006c  008b  009e  0161

could not get driver version for /dev/input/mice, Not a typewriter

For example, some touchscreen event. Any touchscreen press-up or press-down will return a vector of values related with the event (please, see include/linux/input.h for detail)

bash-3.2# getevent /dev/input/event2

0003 0000 0000020e

0003 0001 0000014a

0003 0018 00000037

0001 014a 00000001

0000 0000 00000000

0003 0000 00000209

0003 0001 00000147

Labels (1)
Tags (2)
No ratings
Version history
Last update:
‎08-03-2012 03:50 PM
Updated by: