Adding Voice Support to GUI Guider for i.MX 93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding Voice Support to GUI Guider for i.MX 93

Adding Voice Support to GUI Guider for i.MX 93

The user interface has limited the use of the tool GUI Guider. Getting an interaction only through a mouse or touchscreen can be enough for some use cases. However, sometimes the use case requires to go beyond its limitations. This video/appnote explores the possibility of integrating voice by creating a bridge between a speech recognition technology, such as VIT, and the interface creator GUI Guider. It uses a universal way to link all the voice recognition commands and a wakeword to any interaction created by GUI Guider.

The following video shows the steps necessary to create that connection by creating the voice recognition using VIT voice commands and wakewords, create an interface of GUI Guider using a template, how to connect between them using the board i.MX 93 evk and testing it.

For more information consult the following links

AppNote HTML: https://docs.nxp.com/bundle/AN14270/page/topics/abstract.html?_gl=1*1glzg9k*_ga*NDczMzk4MDYuMTcxNjky...

AppNote PDF: https://www.nxp.com/docs/en/application-note/AN14270.pdf

Associated File: AN14270SW

 

标签 (3)
无评分
版本历史
最后更新:
‎05-28-2024 02:26 PM
更新人: