Adding Voice Support to GUI Guider for i.MX 93

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding Voice Support to GUI Guider for i.MX 93

Adding Voice Support to GUI Guider for i.MX 93

The user interface has limited the use of the tool GUI Guider. Getting an interaction only through a mouse or touchscreen can be enough for some use cases. However, sometimes the use case requires to go beyond its limitations. This video/appnote explores the possibility of integrating voice by creating a bridge between a speech recognition technology, such as VIT, and the interface creator GUI Guider. It uses a universal way to link all the voice recognition commands and a wakeword to any interaction created by GUI Guider.

The following video shows the steps necessary to create that connection by creating the voice recognition using VIT voice commands and wakewords, create an interface of GUI Guider using a template, how to connect between them using the board i.MX 93 evk and testing it.

For more information consult the following links

AppNote HTML: https://docs.nxp.com/bundle/AN14270/page/topics/abstract.html?_gl=1*1glzg9k*_ga*NDczMzk4MDYuMTcxNjky...

AppNote PDF: https://www.nxp.com/docs/en/application-note/AN14270.pdf

Associated File: AN14270SW

 

Labels (3)
No ratings
Version history
Last update:
‎05-28-2024 02:26 PM
Updated by: