Adding Support For a New NAND with i.MX28 on Win CE
Structures to be modified
The main table that needs to be modified is in C:\WINCE600\PLATFORM\COMMON\SRC\SOC\COMMON_FSL_V2_PDK1_9\NAND\INC\NANDTYPES.h. Add the Nand specific information to the following structure.
typedef struct _NandChipInfo
{
FlashInfo fi; //@<<info> FlashInfo structure
BYTE NANDCode[NANDID_LENGTH];//@<<info> NAND full ID
BYTE NumBlockCycles; //@<<info> flash erase address cycle
BYTE ChipAddrCycleNum; //@<<info> flash access address cycle
BYTE DataWidth; //@<<info> 8/16 bits data width
BYTE BBMarkNum; //@<<info> MAX_MARK_NUM = 4
BYTE BBMarkPage[MAX_MARK_NUM];//@<<info> MAX_MARK_NUM = 4
BYTE StatusBusyBit; //@<<info> interleave mode support
BYTE StatusErrorBit; //@<<info> interleave mode support
WORD SpareDataLength; //@<<info> spare area size
BYTE CmdReadStatus; //@<<command> read status
BYTE CmdRead1; //@<<command> read first 256 bytes data
BYTE CmdRead2; //@<<command> read last 256 bytes data
BYTE CmdReadId; //@<<command> read device ID
BYTE CmdReset; //@<<command> reset nand flash
BYTE CmdWrite1; //@<<command> sequence data input
BYTE CmdWrite2; //@<<command> page program
BYTE CmdErase1; //@<<command> block erase
BYTE CmdErase2; //@<<command> block erase
NANDTiming timings; //@<<info> NAND timing parameters
}NandChipInfo, *pNandChipInfo;
All information from NANDCode to CmdErase2, can be obtained from the Nand Datasheet. The structure FlashInfo, is filled in with data obtained from the Nand Analysis sheet. Please check this link to see how to create this spreadsheet from Nand Datasheets.
typedef struct _FlashInfo {FLASH_TYPE flashType;
DWORD dwNumBlocks;
DWORD dwBytesPerBlock;
WORD wSectorsPerBlock;
WORD wDataBytesPerSector;
}FlashInfo, *PFlashInfo;
In the similar way the Nand timings calculated from the spreadsheet are add into this structure.
typedef struct _NANDTiming
{
BYTE DataSetup;
BYTE DataHold;
BYTE AddressSetup;
BYTE DataSample;
}NANDTiming, *PNANDTiming;
Remember to do a clean sysgen and build.
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Report Inappropriate Content
Hi, could you please provide a link to the NAND analysis spreadsheet mentioned in the post. Thanks, Mark