A Patch to Fix the SDMMC Card in L2.6.35_11.09.01_ER UBoot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A Patch to Fix the SDMMC Card in L2.6.35_11.09.01_ER UBoot

A Patch to Fix the SDMMC Card in L2.6.35_11.09.01_ER UBoot

In L2.6.35_11.09.01_ER BSP Uboot, the MMC driver was updated, but there is issue that when you modified some uboot code, the MMC driver has chance to fail to work.

The root cause is that mmc->has_init hasn't been initialized. Sometimes the value will be not zero, then mmc driver will be skipped for initialization. Attached is the patch to fix this issue in L2.6.35_11.09.01_ER BSP Uboot.

Labels (3)
Tags (2)
Attachments
No ratings
Version history
Last update:
‎12-17-2012 07:27 PM
Updated by: