MTBF Data for BGA3023Y

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MTBF Data for BGA3023Y

2,141 Views
harshithram
Contributor II

Hi,

We are using BGA3023Y-1.2GHz 20dB Gain CATV Amplifier in our design. What is the MTBF/Failure rate of that device?

Regards,

Harshith

2 Replies

2,053 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

The BGA3023 is no longer manufacturer and the MTBF is no longer available, all the information about this part is obsolete

BGA3023 Product Information|NXP 

Regards

2,053 Views
harshithram
Contributor II

Thanks Vicente !

--

Regards,

Harshith

From: vicentegomez <admin@community.nxp.com>

Sent: Wednesday, May 13, 2020 3:49 AM

To: Harshithram KV <harshithram@saankhyalabs.com>

Subject: Re: - Re: MTBF Data for BGA3023Y

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MTBF Data for BGA3023Y

reply from Vicente Gomez Salazar

<https://community.nxp.com/people/vicentegomez?et=watches.email.thread>

in *Wireless

Connectivity* - View the full discussion

<https://community.nxp.com/message/1310884?commentID=1310884&et=watches.email.thread#comment-1310884>

0 Kudos
Reply