MCUXpresso - JN5189 - AN1244 missing file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso - JN5189 - AN1244 missing file

Jump to solution
1,064 Views
Larz
Contributor III

Goodday,

I'm on MCUXpresso IDE v11.9.0 [Build 2144] and have JN5189DK6 V2.6.13 installed.

In the Application Notes AN1244 in Section 8.2 is descripted how to change the Touchlink Preconfigured Link Key. See below:

Larz_0-1710406254999.png

The first step is no problem. Just remove the 2 // before the line.

But in the second step you have to change the definition sTLMasterKey in bdb_link_keys.c. This file should be located in BDB\Source\Common. But when I go to: C:\NXP\SDKPackages\JN5189DK6\middleware\wireless\zigbee\BDB\Source\Common\, there is no such file?!?!?

Is the downloaded JN5189DK6 not complete?

Labels (1)
0 Kudos
Reply
1 Solution
997 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

You can find the sTLMasterKey on the app_zps_link_keys.c (Path: SDK\middleware\wireless\zigbee\ZigbeeCommon\Source).

 

Regards,

Ricardo

View solution in original post

0 Kudos
Reply
3 Replies
998 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

You can find the sTLMasterKey on the app_zps_link_keys.c (Path: SDK\middleware\wireless\zigbee\ZigbeeCommon\Source).

 

Regards,

Ricardo

0 Kudos
Reply
1,005 Views
Larz
Contributor III

Nobody?

0 Kudos
Reply
1,030 Views
Larz
Contributor III

Do NXP employees know this?

0 Kudos
Reply