Kinetis-W series which device can support the TSCH (Time Slotted Channel Hopping)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis-W series which device can support the TSCH (Time Slotted Channel Hopping)?

1,347 Views
isaotakashima
Contributor IV

We want to build a network using the TSCH (Time Slotted Channel Hopping).

We interested the Kinetis-W series, which device can support the the TSCH?

Please reply as soon as possible.

Best regards,

Takashima

0 Kudos
Reply
1 Reply

1,131 Views
antonioconcio
NXP Employee
NXP Employee

Hi Takashima,

Please have a look HERE at KW01 Wireless MCU integrating a sub1-GHz Radio.

You can download the KW01 Connectivity Software HERE​​ which includes an 802.15.4 software implementing the IEEE 802.15.4e Time Slotted Channel Hopping(TSCH) MAC services.

You can also find a TSCH application demo for both Coordinator and End Device at the following path once you install the KW01 Connectivity Software:  C:\Freescale\KW01_Connectivity_Software_1.0.0\ConnSw\examples\ieee_802_15_4\MAC_TSCH_Demo.

Please refer to the file "802154MPDAUG,pdf" present in C:\Freescale\KW01_Connectivity_Software_1.0.0\ConnSw\doc  to know how to run the demo.

Hope this helps,

Antonio

0 Kudos
Reply