K32W061/JN5189: Thread support for ‘Enhanced Frame Pending' (EFP)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32W061/JN5189: Thread support for ‘Enhanced Frame Pending' (EFP)?

ソリューションへジャンプ
653件の閲覧回数
ckielstra
Contributor II

Which version of Thread is supported by the current NXP SDK (v2.6.13)?

I'm asking because we want to use the Enhanced Frame Pending (EFP) feature introduced in Thread v1.2.
If already supported by the SDK, then how do we activate this feature?

0 件の賞賛
返信
1 解決策
630件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. The OpenThread middleware is not included on the SDK. You need to get it from the GitHub - NXP/ot-nxp: OpenThread on NXP examples.

 

Please check the information of each release directly: Releases · NXP/ot-nxp · GitHub

 

Regards,

Ricardo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
631件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. The OpenThread middleware is not included on the SDK. You need to get it from the GitHub - NXP/ot-nxp: OpenThread on NXP examples.

 

Please check the information of each release directly: Releases · NXP/ot-nxp · GitHub

 

Regards,

Ricardo

0 件の賞賛
返信