How to send a non-standard packet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to send a non-standard packet?

Jump to solution
1,837 Views
sChameleoNz
Contributor III

I've been using SDK_2_6_4_JN5189DK6.

And I want to send and receive a non-standard 802.15.4 packet while using ZB.

How could I achieve this?

Labels (3)
0 Kudos
Reply
1 Solution
1,824 Views
nxf56274
NXP Employee
NXP Employee

Hi,

It is impossible to send the non-standard 802.15.4 packet. The zigbee frame header and tail is added by the lib that is invisible to us.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,825 Views
nxf56274
NXP Employee
NXP Employee

Hi,

It is impossible to send the non-standard 802.15.4 packet. The zigbee frame header and tail is added by the lib that is invisible to us.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------