wlan 8890 will show interface invaild and can't be connected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wlan 8890 will show interface invaild and can't be connected

719 Views
Mike17
Contributor I

Hi I use 8890 to establish uAP mode , i found that the client will be disconnected  and the FW will dump some information , it shows carrier is off   there anyone know how to fix this?

------------moal_debug_info-------------
Driver version = PCIE9098--17.68.1.p81-MXM5X17277-GPL-(FP68)
main_state = 4
ioctl_pending = 0
tx_pending = 0
rx_pending = 0
lock_count = 45
malloc_count = 49
mbufalloc_count = 136
malloc_cons_count = 4
hs_skip_count = 0
hs_force_count = 0
[Interface : mmlan0]
wmm_tx_pending[0] = 0
wmm_tx_pending[1] = 0
wmm_tx_pending[2] = 0
wmm_tx_pending[3] = 0
Media state = "Disconnected"
carrier off
tx queue 0: stopped
tx queue 1: stopped
tx queue 2: stopped
tx queue 3: stopped
mmlan0: num_tx_timeout = 0
[Interface : muap0]
wmm_tx_pending[0] = 0
wmm_tx_pending[1] = 0
wmm_tx_pending[2] = 0
wmm_tx_pending[3] = 0
Media state = "Disconnected"
carrier off

 

0 Kudos
1 Reply

623 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Mike17,

I would handle this case internally and post the answer in the following thread:

Re: wlan 8890 suspend/resume issue - NXP Community

 

Best Regards,

Alexis Andalon

0 Kudos