iw phy phy0 info
command, I noticed that there is no support for 5GHz frequencies in the output for my region (GB). The AP creation process is failing due to this limitation.
Here are my test setup details:
* 5180 MHz [36] (23.0 dBm) (no IR) * 5200 MHz [40] (23.0 dBm) (no IR) * 5220 MHz [44] (23.0 dBm) (no IR) * 5240 MHz [48] (23.0 dBm) (no IR) * 5260 MHz [52] (20.0 dBm) (no IR, radar detection) * 5280 MHz [56] (20.0 dBm) (no IR, radar detection) * 5300 MHz [60] (20.0 dBm) (no IR, radar detection) * 5320 MHz [64] (20.0 dBm) (no IR, radar detection) * 5500 MHz [100] (26.0 dBm) (radar detection) * 5520 MHz [104] (26.0 dBm) (radar detection) * 5540 MHz [108] (26.0 dBm) (radar detection) * 5560 MHz [112] (26.0 dBm) (radar detection) * 5580 MHz [116] (26.0 dBm) (radar detection) * 5600 MHz [120] (26.0 dBm) (radar detection) * 5620 MHz [124] (26.0 dBm) (radar detection) * 5640 MHz [128] (26.0 dBm) (radar detection) * 5660 MHz [132] (26.0 dBm) (radar detection) * 5680 MHz [136] (26.0 dBm) (radar detection) * 5700 MHz [140] (26.0 dBm) (radar detection) * 5720 MHz [144] (26.0 dBm) (radar detection) * 5745 MHz [149] (23.0 dBm) (no IR) * 5765 MHz [153] (23.0 dBm) (no IR) * 5785 MHz [157] (23.0 dBm) (no IR) * 5805 MHz [161] (23.0 dBm) (no IR) * 5825 MHz [165] (23.0 dBm) (no IR) * 5845 MHz [169] (disabled) * 5865 MHz [173] (disabled)
For other countries' 5GHz AP frequencies are listed, but for GB (United Kingdom) no supporting frequencies are found. I've looked into similar threads, like the one here, where users faced related issues, but their solutions didn't apply to my case.
Thank you in advance for your assistance!
Hi,
Any update on this?
Hello,
Thank you in advance for contacting NXP support.
Can you please help me with the following information in order to have a better understanding of you case:
Please help me with the following information.
@nxf77486 Please find some details,
Please ask if you need any other details