I compiled the rdrw612bga_wifi_cli project and program the firmware to the EVK to run,
but can't scan any wifi networks.
# wlan-scan
Scan scheduled...[wifi] Warn: Scan temporary failure
please check the log.
my questions:
1, Why is mac address 00:00:00:00:00:00 when boot up the demo?
2, I set the mac address using Wlan-Set-Mac command,
but the issue is same.
thanks for your great support in advance.
==========
IDE Version: MCUXpresso IDE v11.9.0_2144
SDK Version: SDK_2_13_3_RD-RW612-BGA
EVK: RD-RW61X-BGA-IPA-2A-V4
Solved! Go to Solution.
Dear @sohu_hakka
It seems that you are using the wrong WiFi firmware.
We have a MAC Address: 00:00:00:00:00:00 when we are trying to run wifi_cli application with a WiFi manufacturing firmware, instead of the production firmware.
Manufacturing firmware (rw61xw_sb_mfg_fw_cpu1_a2.bin) shall only be used with uart_wifi_bridge application and labtool)
The production firmware (rw61x_sb_wifi_a2.bin) shall be used for all other wifi usage.
Please flash SDK 2.13.3 WiFi production firmware with below command on JLink Commander:
loadbin rw61x_sb_wifi_a2.bin,0x08400000
(firmwares are located in mcuxpresso\02\SDKPackages\SDK_2_13_3_RD-RW612-BGA\components\conn_fwloader\fw_bin)
Regards,
Olivier
Thanks, It works.
Dear @sohu_hakka
It seems that you are using the wrong WiFi firmware.
We have a MAC Address: 00:00:00:00:00:00 when we are trying to run wifi_cli application with a WiFi manufacturing firmware, instead of the production firmware.
Manufacturing firmware (rw61xw_sb_mfg_fw_cpu1_a2.bin) shall only be used with uart_wifi_bridge application and labtool)
The production firmware (rw61x_sb_wifi_a2.bin) shall be used for all other wifi usage.
Please flash SDK 2.13.3 WiFi production firmware with below command on JLink Commander:
loadbin rw61x_sb_wifi_a2.bin,0x08400000
(firmwares are located in mcuxpresso\02\SDKPackages\SDK_2_13_3_RD-RW612-BGA\components\conn_fwloader\fw_bin)
Regards,
Olivier