QN9080: unable to program the device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080: unable to program the device.

932 Views
Vasilis
Contributor I

Hello,

In our company we have designed 2 boards that are both using the QN9080-001-M17AZ Bluetooth Module. We have followed the design rules and we are making use of the SWDIO, SWCLK, RESETN and ISP pins with the correct configuration in terms of pins and pull-up/pull-down resistors. However, in neither of these boards are we able to successfully connect to the QN9080 and program it. The MCU_Xpresso is giving an error that the device is not discoverable. 
Is there something we did not take into account? According to the datasheets, there is not anything wrong. Any help is appreciated

Vasilis 

Labels (1)
  • QN

0 Kudos
2 Replies

904 Views
nxf56274
NXP Employee
NXP Employee

Hi,

What is your programmer? Jlink? Check the module's voltage and XTAL. Is the voltage 3.3V? Does the crystal work normally?

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

900 Views
Vasilis
Contributor I

We are using the PEMicro debugging interface. We eventually found 2 issues on some of our boards:

  • Some pins were not soldered correctly, probably to wrong mask used by the PCB manufacturer.
  • The RESETN port should not be connected to the debugger, since it is controlled by the SWDIO port as well.