Problens with ZigBee Pro 3.0 in JN5179

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problens with ZigBee Pro 3.0 in JN5179

1,075 Views
clovisrodrigori
Contributor I

Hi,
we are using in JN5179 the ZigBee PRO Application Template (JN-AN-1229) to develop our product.
In this template the coordinator can creat a network normaly, but, when the router get connected in the network we got a "crash" in this module and after some seconds the coordinator "crash" as well.
Separately both works correctly, the problem happens when both get connected.
In attachmento is the log file with what happens.
Can you help us to fix it? Or, have another template to help us?

 

Ps. We will use the coordinator and router only. We not use end Device in the network.

 

Thanks,

Original Attachment has been moved to: Logs.txt.zip

0 Kudos
6 Replies

678 Views
knguyenning
Contributor I

I got the same problem with version 1002

APP: Power Up
APP: Deleting all records from flash
APP: Application startup
PDM: Segment 36 buffer wear count swap
APP: No event to process
APP: Network Started
APP: Channel - 12
APP: No event to process
APP: vCheckStackEvent: vCheckStackEvent: ZPS_EVENT_NEW_NODE_HAS_JOINED, Nwk Addr=0x19a8

**** Usage fault Handler ****

**** Stack Register Dump ****

R0 = 0x20000268
R1 = 0x191300f2
R2 = 0x81
R3 = 0x0
R12 = 0x2000320a
[Subrou7f24 : 20007f58
20007f28 : 00000000
20007f2c : 00000000
20007f30 : 20007fc8
20007f34 : fffffff9
20007f38 : 20000200
20007f3c : 20007f58
20007f40 : 20003178
20007f44 : 20007f58
20007f48 : 00000000
20007f4c : 20007f58
20007f50 : 200000bc
20007f54 : 00082089
20007f58 : 20000200
20007f5c : 20000100
20007f60 : 00e07a44
20007f64 : fffffff9
20007f68 : 00000000
20007f6c : 20007fa0
20007f70 : 20003100
20007f74 : 00000000
20007f78 : 20002bdc
20007f7c : 000822a3
20007f80 : 0008257a
20007f84 : 61000000
20007f88 : 20003100
20007f8c : 20007fa0
20007f90 : 0008257a
20007f94 : 200000bc
20007f98 : 200000bc
20007f9c : 000822a3
20007fa0 : 00000000
20007fa4 : 20007fa0
20007fa8 : 20003100
20007fac : fffffff9
20007fb0 : 20002a78
20007fb4 : 00000030
20007fb8 : 00000000
20007fbc : e000ed10
20007fc0 : 0008233d
20007fc4 : 00000000
20007fc8 : 200000bc
20007fcc : 200000bc
20007fd0 : 00000208
20007fd4 : 00000000
20007fd8 : 00000000
20007fdc : 00081f7b
20007fe0 : 00000000
20007fe4 : 00081fe9
20007fe8 : 40000004
20007fec : 000000f5
20007ff0 : 000828d4
20007ff4 : 76543210
20007ff8 : fedcba98
20007ffc : e5a498d3


APP: Power Up
APP: Watchdog timer has reset device!

0 Kudos

678 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Khanh,

Are you working with the JN516x?

Could you provide your sniffer log?

Regards,

Mario

0 Kudos

678 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ribeiro,

What is the version of the SDK and the app note that you are using?

Regards,

Mario

678 Views
clovisrodrigori
Contributor I

Hi Mario,

The Sdk version is 7.9.2.

Regards,

0 Kudos

678 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Clovis,

I was checking the JN-AN-1229 and I didn't have any problem with the coordinator and the router.

I downloaded the JN-AN-1229 version 1002.

pastedImage_1.png

Did you modify the application note? What is your application note version?

Best regards,

Mario

0 Kudos

678 Views
clovisrodrigori
Contributor I

Hi Mario, sorry for the delay, I am in vacation.

So, the version is the same yours.

We will download of this from the website again and rebuild all project to get certain that has no modification in the code.

After finish it, I will send the feed back to you.

regards,

Clovis Ribeiro

0 Kudos