PN7462 and PN7362 supporing operating system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 and PN7362 supporing operating system

699 Views
kimhunkt
Contributor I

I want to know if these products support OS.

If there is an OS available, please let us know which OS types are supported.

0 Kudos
1 Reply

695 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @kimhunkt ,

 

Do you mean OS running on the Host which is connected with PN7462/PN7362 ? If yes, any OS can support. For example, if you make a USB CCID device based on PN7462/PN7362, any OS supporting CCID can work with it.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos