MAYA-W1 Bluetooth using Uart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAYA-W1 Bluetooth using Uart

750 Views
Da_123456_DA
Contributor II

Hello,

I'm trying to communicate with my MAYA Bluetooth device

I have connect it to UART9 on my board, setup the device tree correct :

flx4: flexcom@fc018000 {
atmel,flexcom-mode = <ATMEL_FLEXCOM_MODE_USART>;
status = "okay";

uart9: serial@200 {
atmel,use-dma-rx;
atmel,use-dma-tx;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flx4_default>;
status = "okay";
};
 
pinctrl_flx4_default: flx4_uart_default {
pinmux = <PIN_PC28__FLEXCOM4_IO0>,
<PIN_PC29__FLEXCOM4_IO1>;
bias-disable;
};

 

but still can't see the device when I try to use HCITOOL

2 questions:

1. is the config correct?

2. what should be the MAYA pins to allow BT ?

blt_rst = 0 , blt_wkp = 1 pwr_enable=1, wifi_ble_disable = 0

did I miss something ?

 

0 Kudos
8 Replies

681 Views
Da_123456_DA
Contributor II

I'm using SAMA5d27 by Microchip running linux4sam 6.1

I'm trying to run MAYA-W1 BT\Wireless device 

after digging I understand I need to upload the firmware to the device after boot, but I can't seem to understand how to do it

when I connect to the UART port of the MAYA (which use for BT) I can see "Heartbeat" of 3 bytes every 1 seconds.

from google I understand it's waiting to firmware to be upload - but I couldn't find how to upload the image .

also I understand that the firmware is used for both BT and WiFi and I can't work only with BT (this is not mention any where...)

so maybe you know this and can help me with the firmware installtion ?

 

Thanks ,

0 Kudos

670 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Thanks for the reply.

I would recommend you to take a look to this webpage in which you will find more information related to the module and EVK.
Regarding the FW, please take a look to the following GitHub repositories in which you will find Wi-Fi Firmware and Wi-Fi Driver.

 

Regards,

Daniel.

0 Kudos

656 Views
Da_123456_DA
Contributor II

I have done everything it said in the manual

still unable to connect 

just to see I understand correct:

1.The WiFi and the BT work together - there is no only BT firmware ?

2. I must upload to the device the firmware in order to make it work , if I don't do this nothing will work

no BT and no WiFi? so the name "Wifi driver\firmware" is not correct - it should be WiFi&BT firmware?

I think this is confusing .....

3. If I get the "Heartbeat" when I try to connect to the BT using UART - it mean that the device is power, but no firmware is uploaded ?

4. Can it be that the problem is that the SDIO line is not config correct in the Device_Tree? I understand I need to setup the config to support WiFI and not leave it as MMC SDIO ?(this is not written anywhere)

 

Thanks ,

 

0 Kudos

644 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

I’m sorry if I wasn’t clear.

In the FW GitHub I shared with you, in tag lf-6.6.3-1.0.0, if we take IW416 as example and we take a look to the following directory imx-firmware/nxp/FwImage_IW416_SD you will find 3 different firmwares.

 

The one named “sdiouartiw416_combo_v0.bin” will work for both Wi-Fi and BT. Please notice that SDIO will be used for Wi-Fi and UART for BT.

The other 2 FWs, are specific to each protocol.

 

In terms of the driver, it is the same for both Wi-Fi and Bluetooth. We name it WLAN driver or Wi-Fi driver though.

 

I would recommend you to take a look to the Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS. This is available in the IW416 documentation.

Please take a look to the whole document, specially to Section 5 and 6.

 

Please note this guide is for an i.MX8MQ-EVK running the i.MX Linux BSP. But I really think it will help you to clear out most of your doubts.

 

Regards,

Daniel.

0 Kudos

565 Views
Da_123456_DA
Contributor II

OK ,
to summarize
if the SDIO line isn't working - I won't be able to load the bin file to the module , and it won't work.
I need to "play" with the device tree until I will see "HIGH SPEED MMC......." connected to the unit

is this correct ?

so , can I ask from you 2 things:
1. send me a working Device_Tree configuration for the SDIO ( I will try to compare with what I have and see what is wrong )
2. show me the "On" status for the device , meaning : what should be on every pin of the module so it will be "Online" and waiting for upload

I want to make sure there is no Hardware \ power issue

Thanks ,

0 Kudos

526 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

I just tried this with an i.MX 8M Mini EVK running the NXP Linux BSP 6.1.22 using the EVK-MAYA-W161.

I was able to load the drivers and FW correctly, please find my logs:

NXP i.MX Release Distro 6.1-mickledore imx8mqevk ttymxc0

imx8mqevk login:
imx8mqevk login:
imx8mqevk login:
imx8mqevk login: root
root@imx8mqevk:~# uname -r
6.1.22+g66e442bc7fdc
root@imx8mqevk:~# [   19.938640] platform sound-ak4458: deferred probe pending
[   19.944078] platform sound-ak5558: deferred probe pending

root@imx8mqevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[   23.940586] mlan: loading out-of-tree module taints kernel.
[   23.968462] wlan: Loading MWLAN driver
[   23.972989] wlan: Register to Bus Driver...
[   23.977490] vendor=0x02DF device=0x9159 class=0 function=1
[   23.983123] Attach moal handle ops, card interface type: 0x108
[   23.989052] rps set to 0 from module param
[   23.993831] SDIW416: init module param from usr cfg
[   23.998772] card_type: SDIW416, config block: 0
[   24.003318] cfg80211_wext=0xf
[   24.006295] max_vir_bss=1
[   24.008929] cal_data_cfg=none
[   24.011896] ps_mode = 1
[   24.014360] auto_ds = 1
[   24.016821] host_mlme=enable
[   24.019702] fw_name=nxp/sdiouartiw416_combo_v0.bin
[   24.024517] SDIO: max_segs=128 max_seg_size=65535
[   24.029238] rx_work=1 cpu_num=4
[   24.032402] Attach mlan adapter operations.card_type is 0x108.
[   24.039194] wlan: Enable TX SG mode
[   24.042702] wlan: Enable RX SG mode
[   24.048210] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[   24.713415] Wlan: FW download over, firmwarelen=570928 downloaded 570928
[   25.982396] WLAN FW is active
[   25.985391] on_time is 25981284400
[   26.021559] fw_cap_info=0x187ccf03, dev_cap_mask=0xffffffff
[   26.027168] max_p2p_conn = 8, max_sta_conn = 8
[   26.050163] Register NXP 802.11 Adapter mlan0
[   26.057684] Register NXP 802.11 Adapter uap0
[   26.070710] Register NXP 802.11 Adapter wfd0
[   26.077796] wlan: version = SDIW416---16.92.21.p84.3-MM5X16391.p3-GPL-(FP92)
[   26.086672] wlan: Register to Bus Driver Done
[   26.091691] wlan: Driver loaded successfully
root@imx8mqevk:~# [   33.760706] VGEN1: disabling
[   33.764158] VGEN6: disabling


By any chance have you reached U-Blox to talk about this situation?

Regards,

Daniel.

0 Kudos

514 Views
Da_123456_DA
Contributor II

I have found the problem

now everything is working

 

Thank you !!!!!!

 

 

now I can connect to the BT , publish my name - connect to it

now I need to build the app is needed.

thank you

700 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Could you please help me with the following information?

- What host are you using?

- Are you using a custom board?

- What OS version are you using?

- What Wi-Fi FW and driver are you using?

 

Regards,

Daniel.

0 Kudos