Hi there,
I am using FRDM-KW38 in project adv_ext_peripheral_bm,
now I want to do some central behavior in this project,
so I call Gap_StartScanning(); but always return gBleFeatureNotSupported_c,
I think lib.a is different so some API is not supported.
Is there any guideline to teach how to add different lib.a to the using project?
I copy central lib.a from project adv_ext_central to my using project adv_ext_peripheral,
and add lib.a like below, it seems not working well.
When Using Gap_StartScanning(); still return gBleFeatureNotSupported_c.
Hello,
Hope you are doing well. I would recommend checking the Wireless UART example. This example implements both the GATT client and server for the custom Wireless UART profile and services.
This example might be helpful for your application, as it can change from a central to peripheral mode.
Hope this helps.
Regards,
Ricardo
Hi @Ricardo_Zamora,
Thanks for reply,
I will try Wireless UART example,
but is there any easier way to add lib.a to my using project?
Regards,
Adam