JN518x: user area in "pFlash"?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JN518x: user area in "pFlash"?

跳至解决方案
1,218 次查看
usaygo
Contributor III

Hello,

We need to store small (16bytes x 3) data at production stage. Normal flash is not good for use because it's easily rewitten. The "pFlash" area is usable place, I think. However pFlash memory map defined in "rom_psector.h" does not seem to have space for generic use.

        struct
        {
            uint32_t rom_patch_region_sz;
...
            uint32_t qspi_app_search_granularity;

            uint32_t reserved1[2];

            uint8_t ISP_protocol_key[16];        /*!< ISP protocol key: key used to encrypt messages over ISP UART
                                                  * with secure access level
                                                  */
            uint64_t ieee_mac_id1;               /*!< IEEE_MAC_ID_1 (Used to over-ride MAC ID_1 in N-2 page) */
            uint64_t ieee_mac_id2;               /*!< IEEE_MAC_ID_2 if second MAC iID is required */

            uint64_t ble_mac_id;                 /*!< BLE device address : only 6 LSB bytes are significant */
            uint8_t  reserved2[104];             /*!< Reserved for future use  */

            uint64_t customer_id;                /*!< Customer ID, used for secure handshake */
            uint64_t min_device_id;              /*!< Min Device ID, used for secure handshake - Certificate compatibility  */
            uint64_t device_id;                  /*!< Device ID, used for secure handshake */
            uint64_t max_device_id;              /*!< Max Device ID, used for secure handshake - Certificate compatibility  */
            uint8_t unlock_key[256];             /*!< 2048-bit public key for secure handshake
                                                  * (equivalent to ‘unlock’ key). Stored encrypted,
                                                  * using the AES key in eFuse*/
        } pFlash;

 

Question1: So far, reserve2[104] is the candidate for the purpose. Please let me know if I should use this area and the future risks if I use the area. Or is there another better area?

Question2: I think the customer_id to unlock_key is provided for the encryption procedure, will it be used by ZigBee PRO or Thread? (we normally use MMAC, not use ZigBee/Thread).

Thanks in advance.

 

0 项奖励
回复
1 解答
1,155 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @usaygo,

Normal flash is not good for us because it's easily rewritten.

Depending on your application, you could secure your device and with that avoid the rewrite without authorization.

Question1: So far, reserve2[104] is the candidate for the purpose. Please let me know if I should use this area and the future risks if I use the area. Or is there another better area?

Sure you could use this section for saving your data. Just be sure and do not modify the config values.

Question2: I think the customer_id to unlock_key is provided for the encryption procedure, will it be used by ZigBee PRO or Thread? (we normally use MMAC, not use ZigBee/Thread).

In this case, the customer ID is for the 802.15.4 protocol, and the unlock key is in the case that you want to lock your device.

Regards,

Mario

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,156 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @usaygo,

Normal flash is not good for us because it's easily rewritten.

Depending on your application, you could secure your device and with that avoid the rewrite without authorization.

Question1: So far, reserve2[104] is the candidate for the purpose. Please let me know if I should use this area and the future risks if I use the area. Or is there another better area?

Sure you could use this section for saving your data. Just be sure and do not modify the config values.

Question2: I think the customer_id to unlock_key is provided for the encryption procedure, will it be used by ZigBee PRO or Thread? (we normally use MMAC, not use ZigBee/Thread).

In this case, the customer ID is for the 802.15.4 protocol, and the unlock key is in the case that you want to lock your device.

Regards,

Mario

0 项奖励
回复
1,146 次查看
usaygo
Contributor III

Hello Mario,

Your answer is really appreciate.

Thank you very much!

0 项奖励
回复