JN5169 can not programed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5169 can not programed

2,322 Views
yuchenglin
Contributor II

Hello, I use JN5169 to design a product, which has been mass produced many times. This time, there are a batch of jn5169, more than 1000 of which cannot be programed (programing with jn51xxprogrammer.exe). The chip number is JN5169 SBR234 ZSD5451. They chip supplier said that this batch was befort 2015. Is there any special requirements for programming  JN5169 which before 2015?

  I am looking forward to your reply, thank you.

0 Kudos
16 Replies

2,287 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yuchenglin,

Please look at the following community post that could help you with the programming issues.

Solving Problems in Reading/Flashing JN516x Modules

Please let me know your findings.

Regards,

Mario

0 Kudos

2,277 Views
yuchenglin
Contributor II

thanks for your reply. the programming operation I'am very clear. because the other JN5169 (which tail number is not ZSD5451) is programed sucessful. But the JN5169 which number is  JN5169 SBR234 ZSD5451 can't be programed.

     There is more than 1000 piece of Jn5169 which number is N5169 SBR234 ZSD5451 in my hand.so I need your help urgently, thank you!

0 Kudos

2,257 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yuchenglin,

I am not sure where you bought this part number.

Could you please share the link about this JN5169? It seems that is not part of the NXP products, I need to check the marking of the device.

Regards,

Mario

0 Kudos

2,237 Views
yuchenglin
Contributor II

hello,I share the link about JN5169 bellow, I am waitting for your reply,  thank you!

https://www.nxp.com/products/wireless/zigbee/zigbee-and-ieee802-15-4-wireless-microcontroller-with-5...

0 Kudos

2,244 Views
usaygo
Contributor III

Hello,

The "JN5169 SBR234 ZSD5451" seems JN5169 (chip model) with lot number "SBR234 ZSD5451". As long as I know, JN5169 does not have many variations (-001A, -001Z).

We also use thousands of JN5169 and this issue is also sensitive to us. We hope this to be identified sooner.

Thanks!

0 Kudos

2,226 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @usaygo,

You are right there are not a lot of variations for the JN5169. So, the programming process should be the same,

How are you connect the module that you have? Could you please share some images of the module that you have?

If The "JN5169 SBR234 ZSD5451"  has an internal JN5169 from us, the process is the same, just please be sure that you are entering program mode.

Regards,

Mario

0 Kudos

2,199 Views
yuchenglin
Contributor II

thanks for your reply. the programming operation I'am very clear. because the other JN5169 (which tail number is not ZSD5451) is programed sucessful. But the JN5169 which number is  JN5169 SBR234 ZSD5451 can't be programed.
     There is more than 1000 piece of Jn5169 which number is N5169 SBR234 ZSD5451 in my hand.so I need your help urgently, thank you!

0 Kudos

2,188 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yuchenglin,

Where did you buy the JN5169 SBR234 ZSD5451?

If this custom module has the JN5169 from NXP should be programmed as the JN5169 that we provide.

Could you please share an image of the module? Do you have the schematic? Do you have access to the programming pins?

Regards,

Mario

0 Kudos

2,160 Views
yuchenglin
Contributor II

I bought the JN5169 SBR234 ZSD5451 from one of the local dealers,my schematic and my programming operation are absolutely right,because the replacement other JN5169 (which tail number is not ZSD5451)in the same board is programed sucessful.Can you check the JN5169 SBR234 ZSD545 is anything special about this chip?
Is the chip is otp? or it's programming port is disable? or this chip is fake? there is some image about my borad bellows

yuchenglin_0-1635210078809.png

 

yuchenglin_1-1635210237676.png

 

0 Kudos

2,155 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yuchenglin,

Can you check the JN5169 SBR234 ZSD545 is anything special about this chip?

It is weird because it is not part of our products, I am checking this IC, and get back to you as soon as possible.

Regards,

Mario

0 Kudos

2,147 Views
yuchenglin
Contributor II

yuchenglin_0-1635227456762.png

I have more than 1000 pieces of JN5169 SBR234 ZSD5451 on my hands. and none of them  can be programed. the image above is the picture of the chip. so the problem is serious!!!I need your help, thank you!

0 Kudos

2,130 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

It seems to be correct, but the UART programming process is the same.

Is it possible that you could share where you bought or what is the distributor that you asked for this device?

Regards,

Mario

0 Kudos

2,022 Views
yuchenglin
Contributor II
 

yuchenglin_1-1635555514159.png

 

The JN5169 where I bought  is Shenzhen meisixing Technology Co., Ltd.The seller  could not tell me the distributor. According the chip number can you check any problem?

1,980 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yuchenglin,

I looked into this company that provides the JN5169 Devices. The Shenzhen meisixing Technology Co., Ltd is not authorized to provide this product.

We do not encourage you to buy from a non-authorized distributor.
If you do so then you will not have any support from NXP. Even if they are not counterfeit. We cannot guarantee something we don't know how it was handled or the origin of the parts.

Sorry for any inconvenience that this may cause you.

Regards,

Mario

0 Kudos

2,211 Views
usaygo
Contributor III

Hello Mario,

I'm just an observer. Sorry for confusing you. So far, I don't have the same problem. (Some chips are OTP programmed to be write protected???)

Thanks!

0 Kudos