JN5168 - Synchronize Between 2 devices (router-router/router-end device)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5168 - Synchronize Between 2 devices (router-router/router-end device)

435 Views
fehnrirx
Contributor I

I need to know how to synchronize between 2 devices, light switch for example, where when i turn switch 1, it also turn on the switch 2, and so on. or at least the main switch will change it state whether the secondary switch is used. the purpose is like 2-way switch, where i can control the light with these switch. my base code is using JN-AN-1189. thanks

Tags (2)
0 Kudos
1 Reply

260 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi William,

If a controller node is bound to one or more light nodes The lights will be controlled synchronously.

I recommend you take a look at the JN-AN-1189-ZigBee-HA-Demo-1v15.pdf

Chapter: 6.2.2 Commissioning Light Nodes - Binding

Please follow the next path.C:\NXP\bstudio_nxp\workspace\JN-AN-1189-ZigBee-HA-Demo\Doc

Regards,

Mario

0 Kudos