Hi.
I was wondering the real amount of "maximum number of nodes" on a star topology by using the JN5168-001-M06, in other words, without using any router. Zigbee PRO Stack datasheet doesn't specify a maximum value for this parameter. As I'm concerned, this is related to RAM usage and configuration of another parameter values.
So:
1) There's a fixed maximum amount of "Maximum Number of Nodes"?
2) If this value depends on other values, how can i calculate the parameter? Otherwise, there is any documentation related to this?
@mario_castaneda hope you can help me in this one. Regards!
Solved! Go to Solution.
Hello @ffonck
Hope you are doing well.
As indicated in Zigbee 3 Stack User Guide, Chapter 1 Overview, Section 1.2 ZigBee PRO Network Topology, the stack is designed primarily for Mesh networks. Please, consider the following parameters:
Neighbour Table:
Child Table Size:
Address Map Table
MAC Address Table
Routing Table
Regards,
Eduardo.
Thanks for the useful information. I'll have this consider for future developments.
Hello @ffonck
Hope you are doing well.
As indicated in Zigbee 3 Stack User Guide, Chapter 1 Overview, Section 1.2 ZigBee PRO Network Topology, the stack is designed primarily for Mesh networks. Please, consider the following parameters:
Neighbour Table:
Child Table Size:
Address Map Table
MAC Address Table
Routing Table
Regards,
Eduardo.