Hi @nxp
In JN-AN-1245 the CoinCell Example for JN5189 is missing. It is mentioned in the documents but the actual source directories are empty.
Could you provide this?
So far I successfully implemented my zigbee application using the DimmerSwitch Example included in JN-AN-1245 and would like to take the next step by switching to the CoinCell Example as my pcb is only driven by a CoinCell.
Thank you.
BR
Matthias
Hi @matthias_brand,
I hope you are doing.
I send you a message internally for the requested code.
Regards,
Mario
I'm working on the JN-AN1246 example and now I want to shift my circuit to coin cell. Can you please send me a coin cell example?
Regards,
Talha
Hi Matthias,
I am sorry for my late reply. I am working on the code that you are requesting.
Regards,
Mario
@mario_castaneda any update?
Hi @matthias_brand,
I hope you are doing great. Did you download the AN from the JN5189/88? What are the directories that you are seeing empty?
Then, you could define the #ifdef CoinCellSwitch to enable the coin cell feature.
Let me know if you have any other questions.
Regards,
Mario
I downloaded it via https://www.nxp.com/webapp/sps/download/license.jsp?colCode=JN-AN-1245.
The archive contains the following directories:
Directory of C:\Users\matth\Downloads\JN-AN-1245 (1)\JN-AN-1245
17/08/2020 03:58 <DIR> .
17/08/2020 03:58 <DIR> ..
17/08/2020 03:56 <DIR> Binaries
17/08/2020 03:57 <DIR> ColorSceneController
17/08/2020 03:57 <DIR> Common
17/08/2020 03:56 <DIR> Common_Controller
17/08/2020 03:55 <DIR> Common_Switch
17/08/2020 03:56 <DIR> DimmerSwitch
17/08/2020 03:56 <DIR> Doc
17/08/2020 03:55 <DIR> GpEhSwitch
17/08/2020 03:56 <DIR> mcux
17/08/2020 03:57 <DIR> NFC
17/08/2020 03:57 <DIR> RemoteControlGUI
14/08/2020 05:37 5 Version.txt
1 File(s) 5 bytes
13 Dir(s) 43.626.840.064 bytes free
Thereby the directories "CoinCellSwitch" and "Common_CoinCellSwitch "are missing.
BR
Matthias