Hello~
I am developing a product using NXP's i.MX RT1052 and Murata's 1ZM (88W8987) module.
In the service scenario, there is a part that communicates with the user's mobile phone using the SPP function of Bluetooth classic.
My device(server) <-> Smartphone(client)
Through the example included in the SDK, it was confirmed that communication based on the standard UUID (00001101-0000-1000-8000-00805f9b34fb) is possible.
The problem is that if a custom UUID is applied, communication is not possible.
I checked that the custom UUID is applied by calling the BT_dbase_change_attr_value() function, but it is failing in the spp connection stage.
Is SPP communication possible by applying a custom UUID?
Please help answer the above queries as soon as possible.
Thanks and Regards,
Kisoo Lee