ERROR: Function failed: do_configure (log file is located at /warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/temp/log.do_configure.12645

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR: Function failed: do_configure (log file is located at /warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/temp/log.do_configure.12645

7,141 Views
nayananr
Contributor I

Hi,

I am working on warp7 wifi module, while building an image i am getting Feature failure for do_configure, Can any one help me how to solve this? I am using bitbake core-image-base command to build the image.

 

i have attached error log bellow, i have attached .pdf file that i used to build the image for warp7 .

 

Thanks and Regards

Nayana

Original Attachment has been moved to: errorlog.zip

0 Kudos
2 Replies

3,302 Views
texierp
Contributor III

Hi,

Try to clean the package:

bitbake -c cleansstate kmod-native

and relaunch your build.

Regards

PJ

0 Kudos

3,302 Views
nayananr
Contributor I

Hi Pierre,

As you suggested i executed bitbake -c cleansstate kmod-native and again i proceeded with building image by using bitbake core-image-base but i got same error while building an image.

i have attached error log bellow:

warp7/fsl-community-bsp/build1$ bitbake -c cleansstate kmod-native
Loading cache: 100% |##########################################################################################################| ETA: 00:00:00
Loaded 2200 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx7s-warp"
DISTRO = "poky"
DISTRO_VERSION = "2.1.3"
TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "heads/remotes/yocto/master:50fdd784231299bedb008f20adeaeeca3eb1452d"
meta-oe
meta-multimedia = "HEAD:55c8a76da5dc099a7bc3838495c672140cedb78e"
meta-fsl-arm = "HEAD:e2254e7b2ded0c2b66b1226f879b3a6d52037b2d"
meta-fsl-arm-extra = "HEAD:2c28e636ec15c2cfd49bc9cebe0bbbcfde95bc7b"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"

NOTE: Preparing RunQueue
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 2 tasks of which 0 didn't need to be rerun and all succeeded.
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$
ee209700@pcz-ee209700:/u/ee209700/warp7/fsl-community-bsp/build1$ bitbake core-image-base
Loading cache: 100% |##########################################################################################################| ETA: 00:00:00
Loaded 2200 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx7s-warp"
DISTRO = "poky"
DISTRO_VERSION = "2.1.3"
TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "heads/remotes/yocto/master:50fdd784231299bedb008f20adeaeeca3eb1452d"
meta-oe
meta-multimedia = "HEAD:55c8a76da5dc099a7bc3838495c672140cedb78e"
meta-fsl-arm = "HEAD:e2254e7b2ded0c2b66b1226f879b3a6d52037b2d"
meta-fsl-arm-extra = "HEAD:2c28e636ec15c2cfd49bc9cebe0bbbcfde95bc7b"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: kmod-native-22+gitAUTOINC+42f32b8ae4-r0 do_unpack: kmod-native: the directory ${WORKDIR}/git (/u/ee209700/warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/git) pointed to by the S variable doesn't exist - please set S within the recipe to point to where the source has been unpacked to


ERROR: kmod-native-22+gitAUTOINC+42f32b8ae4-r0 do_configure: Function failed: do_configure (log file is located at /u/ee209700/warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/temp/log.do_configure.5801)
ERROR: Logfile of failure stored in: /u/ee209700/warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/temp/log.do_configure.5801


Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: Executing shell function autotools_preconfigure
| DEBUG: Shell function autotools_preconfigure finished
| DEBUG: Executing python function autotools_copy_aclocals
| DEBUG: Python function autotools_copy_aclocals finished
| DEBUG: Executing shell function do_configure
| gtkdocize: neither configure.ac nor configure.in exist


| touch: cannot touch '/u/ee209700/warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/git/libkmod/docs/gtk-doc.make': No such file or directory
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /u/ee209700/warp7/fsl-community-bsp/build1/tmp/work/x86_64-linux/kmod-native/22+gitAUTOINC+42f32b8ae4-r0/temp/log.do_configure.5801)
ERROR: Task 412 (/u/ee209700/warp7/fsl-community-bsp/sources/poky/meta/recipes-kernel/kmod/kmod-native_git.bb, do_configure) failed with exit code '1'


NOTE: Tasks Summary: Attempted 890 tasks of which 879 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:

Thanks and Regards

Nayana

0 Kudos