Does KW41z support 8 BLE Peripheral connection concurrently?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does KW41z support 8 BLE Peripheral connection concurrently?

1,140 Views
mayank_sharma1
Contributor III

Hi,

I am evaluating BLE v4.2 on KW41z module.

Does BLE stack on this module in Central mode support 8 simultaneous peripheral connections in round robin mode?

For example, Central connects to each peripheral once and iterates over them at rate of 7.5 milliseconds of connection interval.

Regards,

Mayank

Labels (2)
3 Replies

549 Views
miguel_reyes
NXP Employee
NXP Employee

Hi mayanksharma‌,

No, KW41Z supports up to 2 simultaneous hardware connections. 

549 Views
jcolyn
Contributor I

Hi,

Could you tell me the reasoning behind only being able to have two simultaneous connections on the KW41Z?

Is it due to memory limitations?

0 Kudos

549 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jaco,

The KW41z was designed for support up to 2 simultaneous hardware connections.

But if you are looking for a design that support more than 2 simultaneous connections you can take a look to the QN9020.

Ultra low power Bluetooth LE system-on-chip solution|NXP 

QN9020 is in  the Central role, it shall support eight connections at the same time.

Best Regards,

Mario