Does 88Q9098 support 802.11d?Why don‘t 88Q9098 support it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does 88Q9098 support 802.11d?Why don‘t 88Q9098 support it?

537 Views
LewisLiu
Contributor III
 
Labels (2)
0 Kudos
2 Replies

492 Views
LewisLiu
Contributor III

Hi Olivier,

 Thank you for your help!

Best Regards,

Lewis

0 Kudos

522 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @LewisLiu 

88Q9098 supports 802.11d, but it needs to be configured.

 

Could you please provide details on your setup ?:

- host used

- host OS (Linux/RT/other)

- Wifi SW version

- use case (STA / AP mode)

 

For instance, if using Linux/AP case, you need to define the following parameters in hotstapd.conf: 

- country_code

- ieee80211d=1

 

If using RT platform, the following APIs are available in the i.MX RT SDK:

- wlan_enable_11d()

- wlan_set_country

 

Regards,

Olivier