Hi Olivier,
Thank you for your help!
Best Regards,
Lewis
Dear @LewisLiu
88Q9098 supports 802.11d, but it needs to be configured.
Could you please provide details on your setup ?:
- host used
- host OS (Linux/RT/other)
- Wifi SW version
- use case (STA / AP mode)
For instance, if using Linux/AP case, you need to define the following parameters in hotstapd.conf:
- country_code
- ieee80211d=1
If using RT platform, the following APIs are available in the i.MX RT SDK:
- wlan_enable_11d()
- wlan_set_country
Regards,
Olivier