Continuous TX modes for testing, analysis, certification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Continuous TX modes for testing, analysis, certification

1,078 Views
thomasblank
Contributor II

Hi,

We need to put the KW41Z SoC into different continuous TX modes for testing purposes.

In the SMAC-Connectivity test example there are continuous modes with an unmodulated carrier and different modulated carriers. Looking through the code of that example I found the function ASP_TelecTest ins line 580 of the file MKW41Z_ConnSw_1.0.2\middleware\wireless\ieee_802_15_4_5.3.2\phy\source\MKW41Z\ASP.c. The test mode is set in the function TestMode in line 2596 in the file MKW41Z_ConnSw_1.0.2\middleware\wireless\smac_3.3.2\examples\connectivity_test\Connectivity_TestApp.c

Question 1: A possible test mode that the TestMode function might set is gTestContinuousTxContPN9_c. In the switch statement in ASP_TelecTest there is no case gTestContinuousTxContPN9_c. Which registers do I need to set how in a KW41Z SoC to send a continuous, randomly modulated signal?

Question 2: In the other cases in ASP_TelecTest, the code sets the register XCVR_MISC->DTEST_CTRL. In memory, that would be the address 4005C29C. That register is not documented in the MKW41Z/31Z/21Z Reference Manual. It should be on page 1909, but it's not there. Where can I get documentation about that register?

Regards,

Thomas

Labels (2)
Tags (1)
0 Kudos
2 Replies

713 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Thomas Blank

About your questions

Yes, I have checked the example code of connectivity test and you are right, gTestContinuousTxContPN9_c is not implemented in the example. But if you want to test this mode, I can recommend you to use the black box example from ieee_802_15_4, here is already implemented. You can use radio test feature from test tool software which offers same functionality. You can find a window as the following;

pastedImage_1.png

Hope this information could help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

713 Views
mangramarco
Contributor III

Hello, i need to solve the same issue but in my version of test tool i've not kw41z tab. How can i add it?

thank you 
Marco

0 Kudos