CW example code for QN9030THN/001Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW example code for QN9030THN/001Z

470 Views
TBone123
Contributor I

I need a simple CW code for 2.45GHz with the latest(?) SDK for antenna test.

Anyone has suggestion?

Labels (1)
0 Kudos
1 Reply

428 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @TBone123,

I hope you are doing good! Please help me taking a look into the RF System Evaluation Report for the QN9090 as reference for testing the QN9030, as there are various tests and setups worth noting (3.3.2 TX with continuous transmission makes use of CW).

For some custom tests, the black box examples is available for RF testing, as it enables the user to have a way to control the radio through serial commands. The tests in the RF System Evaluation Report could be recreated with the BB examples.

There is a BLE Demo Application User's Guide for demonstration of FSCI  & HCI Blackbox under the SDK Archive documentation:

SDK9030>docs>wireless>Bluetooth>Bluetooth Low Energy Demo Applications User's Guide

Please make sure you are utilizing QN9030's software for these tests, as there are some notable changes between products.

I hope you find this helpful!

Best regards, Julián.

0 Kudos