Hi,
here is my environment
Board : i.MX8MQ Custom Board
Linux version : 6.1.36
Wi-Fi / BT module : QCNFA364A Wi-Fi 5 @ PCIe / BT 4.1 @ USB
When I use bluetooth to connect devices, it would appear a2dp-sink / a2dp-source error. Then it cannot connect any devices.
I found that it seems related with pulseaudio-module. If I use any $ pactl command, it would appear "[drm] pclkc 0 is not supported!" at first time.
Then Bluetooth can connect with devices correctly. Is there anyone know this problem?
Thanks & Regards,
Derek Lin
Hi Derek0902,
I am sorry, since I am working on NXP wifi+bt combo chipsets support only, I can't support you more on this topic.
You should continue with Qualcomm help and/or NXP i.Mx support via host dedicated forum https://community.nxp.com/t5/i-MX-Forums/ct-p/imx-processors.
Regards
Hi,
I see that QCNFA364A = Qualcomm Atheros wifi+bt combo chipset (https://fccid.io/2AOJ9-7357622/User-Manual/USER-MANUAL-rev1-3719936.pdf).
So you should ask for support on Qualcomm community forum.
Nevertheless, since you are running Linux on i.MX8MQ + BT, did you have a look at i.MX8MQ dedicated doc Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual ?
Maybe it will help you.
https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/The-A2DP-Audio-Configuration-Based-On-8... may also help you even if based on i.Mx8MN + NXP 88W8987
Hi @cdoumenc ,
I found that it need to start Pulseaudio, Bluetooth connection would be correct. After I use this command below.
$ /usr/bin/pulseaudio --start --log-target=syslog
Then there are a2dp-sink / a2dp-source registered in Bluetooth.service.
But, as long as it is any command about Pulseaudio, it can make "Endpoint registered" in Bluetooth.service. I think it is weird. Dose the Pulseaudio need to be started manually?
Thanks & Regards,
Derek Lin